6.23.21 putwchar Function
Writes a wide character to stdout.
Include
<wchar.h>
Prototype
wint_t putwchar(wchar_t c);
Arguments
c- the wide character to write
Return Value
The function returns a copy of the wide character written. If a write or encoding error
occurs, WEOF is returned.
Remarks
The function writes the wide character, c, to stdout and at
the position indicated by the file position indicator for the stream (if defined), advancing
the indicator appropriately. The error indicator for stdout will be set on a
write error. If an encoding error occurs, errno is set to the value of the
EILSEQ macro.
Example
#include <wchar.h>
int main(void)
{
wint_t wc;
for(wc = L'0'; iswdigit(wc); wc++)
putwchar(wc);
putwchar(L'\n');
}
Example Output
Content of afile.
0123456789