6.23.45 wcsrtombs Function
Convert a wide character string to a multibyte character sequence.
Include
<wchar.h>
Prototype
size_t wcsrtombs(char * restrict dst, const wchar_t ** restrict src,
size_t len, mbstate_t * restrict ps);
Arguments
dst- a pointer to the object to hold the converted multibyte character sequence
src- the wide character sequence to convert
len- the maximum number of multibyte characters to store
ps- a pointer to a
mbstate_tobject that holds the current conversion state
Return Value
The function returns the number of bytes in the multibyte character sequence, not including
the terminating null character (if any). If src cannot be converted to a
mutlibyte character sequence, (size_t)(-1) is returned.
Remarks
The function converts a wide character string indirectly pointed to by src
beginning in the conversion state, described by the object pointed to by ps,
into a sequence of corresponding multibyte characters, storing the converted characters
(including a terminating null character) into the array pointed to by dst,
provided dst is not a null pointer. Conversion stops when encountering a wide
character that cannot be converted, or when len multibyte characters have
been stored. Each conversion takes place as if by a call to the wcrtomb()
function. By having the argument to specify the current conversion state, this function is
restartable.
An encoding error occurs if src is not a valid multibyte character sequence,
when the function stores the value of the macro EILSEQ in
errno, and the conversion state is unspecified.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <wchar.h>
#include <locale.h>
int main(void) {
const wchar_t * ws = L"Volume: 2L±0.5mL";
char buffer [20];
size_t length;
mbstate_t mbs;
setlocale(LC_CTYPE, "");
mbrlen (NULL, 0, &mbs); /* initialize mbs */
length = wcsrtombs(buffer, &ws, 20, &mbs);
wprintf(L"multibyte string \"%s\" has length %d\n", buffer, length);
}
Example Output
multibyte string "Volume: 2L±0.5mL" has length 17