6.23.46 wcsspn Function
Calculate the number of consecutive wide characters at the beginning of a wide string that are contained in a set of wide characters.
Include
<wchar.h>
Prototype
size_t wcsspn(const wchar_t * s1, const wchar_t * s2);
Arguments
s1- the wide string in which to search
s2- the wide characters to search for
Return Value
Returns the length of the segment in s1 containing wide characters found in
s2.
Remarks
This function will determine the number of consecutive wide characters from the beginning of
the wide string s1 that are contained in the wide string s2.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <wchar.h>
int main(void)
{
wchar_t ws1[20] = L"hello";
wchar_t ws2[20] = L"aeiou";
wchar_t ws3[20] = L"animal";
wchar_t ws4[20] = L"xyz";
int res;
res = wcsspn(ws1, ws2);
wprintf(L"wcsspn(\"%ls\", \"%ls\") = %d\n", ws1, ws2, res);
res = wcsspn(ws3, ws2);
wprintf(L"wcsspn(\"%ls\", \"%ls\") = %d\n", ws3, ws2, res);
res = wcsspn(ws3, ws4);
wprintf(L"wcsspn(\"%ls\", \"%ls\") = %d\n", ws3, ws4, res);
}
Example Output
wcsspn("hello", "aeiou") = 0
wcsspn("animal", "aeiou") = 1
wcsspn("animal", "xyz") = 0