6.23.58 wmemchr Function
Locates the first occurrence of a wide character in part of a wide string.
Include
<wchar.h>
Prototype
wchar_t *wcschr(const wchar_t *s, wchar_t c, size_t
n);
Arguments
s- the wide string in which to search
c- the wide character to search for
n- the number of wide character to search
Return Value
The function returns a pointer to the wide character, or a null pointer if the wide character was not found.
Remarks
The function locates the first occurrence of the wide character c in the
first n wide characters in the wide string pointed to by s.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <wchar.h>
int main(void)
{
wchar_t ws[50] = L"What time is it?";
wchar_t ch1 = L'i', ch2 = L'y';
wchar_t * ptr;
int res;
wprintf(L"ws : %ls\n\n", ws);
ptr = wmemchr(ws, ch1, 50);
if (ptr != NULL)
{
res = ptr - ws + 1;
wprintf(L"%lc found at position %d\n", ch1, res);
}
else
wprintf(L"%lc not found\n", ch1);
wprintf(L"\n");
ptr = wmemchr(ws, ch2, 50);
if (ptr != NULL)
{
res = ptr - ws + 1;
wprintf(L"%lc found at position %d\n", ch2, res);
}
else
wprintf(L"%lc not found\n", ch2);
}
Example Output
ws : What time is it?
i found at position 7
y not found