6.23.22 ungetwc Function
Pushes a wide character back to an input stream.
Attention: This function is implemented
only by MPLAB XC32 C compilers.
Include
<wchar.h>
Prototype
wint_t ungetwc(wint_t c, FILE *stream);
Arguments
c- the wide character to push back
stream- the stream to accept the wide character
Return Value
The function returns the wide character pushed back, or WEOF if the
operation fails.
Remarks
The getwc() function is equivalent to fgetwc().
Example
#include <wchar.h>
#include <stdio.h>
int main(void)
{
FILE * myfile;
wint_t wc;
wchar_t buffer[256];
myfile = fopen("afile", "rt");
if(myfile!=NULL)
while(!feof (myfile)) {
wc=getwc(myfile);
if (wc != WEOF) {
if (iswlower(wc)) // is the first wide char lower case
ungetwc(towupper(wc), myfile); // make it upper case
else
ungetwc(wc, myfile);
fgetws(buffer, 255, myfile);
fputws(buffer, stdout);
}
}
}
Example Input
Content of afile.
The curious CASE of this File
the button on the Shirt
The function of this task
Example Output
The curious CASE of this File
The button on the Shirt
The function of this task