6.23.32 wcscat Function
Concatenate a wide string with another.
Attention: This function is implemented
only by MPLAB XC32 C compilers.
Include
<wchar.h>
Prototype
wchar_t * wcscat( wchar_t * restrict s1, const wchar_t * restrict
s2);
Arguments
s1- the wide string to append to
s2- the wide string to append
Return Value
A copy of s1.
Remarks
The function writes a copy of the wide string pointed to by s2 (including
the terminating null wide character) to the location of the null wide character at the end of
the wide string pointed to by s1.
Example
#include <wchar.h>
int main(void)
{
wchar_t ws[40] = L"A long";
wcscat(ws, L" time ago...");
wprintf(L"the complete wide string is \"%ls\"\n", ws);
}
Example Output
the complete wide string is "A long time ago..."