6.23.35 wcscoll Function
Compare two wide strings based on current locale.
Include
<wchar.h>
Prototype
int wcscoll(const wchar_t * restrict s1, const wchar_t * restrict
s2);
Arguments
s1- one wide string to compare
s2- the other wide string to compare
Return Value
Returns a positive integer if s1 is greater than s2, zero
if s1 is equal to s2 or a negative number if
s1 is less than s2.
Remarks
The function returns a value based on the first wide character that differs between
s1 and s2. Wide characters that follow a null wide
character are not compared.
The comparison is based on the LC_COLLATE category of the current locale. As
MPLAB XC8 does not implement locales, wcscoll() is equivalent to
wcscmp() for that implementation.
Example
#include <wchar.h>
int main(void)
{
wchar_t buf1[50] = L"Where is the time?";
wchar_t buf2[50] = L"Where did they go?";
wchar_t buf3[50] = L"Why?";
int res;
wprintf(L"buf1 : %ls\n", buf1);
wprintf(L"buf2 : %ls\n", buf2);
wprintf(L"buf3 : %ls\n\n", buf3);
res = wcscoll(buf1, buf2);
if (res < 0)
wprintf(L"buf1 comes before buf2\n");
else if (res == 0)
wprintf(L"buf1 and buf2 are equal\n");
else
wprintf(L"buf2 comes before buf1\n");
wprintf(L"\n");
res = wcscoll(buf1, buf3);
if (res < 0)
wprintf(L"buf1 comes before buf3\n");
else if (res == 0)
wprintf(L"buf1 and buf3 are equal\n");
else
wprintf(L"buf3 comes before buf1\n");
wprintf(L"\n");
res = wcscoll(L"Why?", buf3);
if (res < 0)
wprintf(L"\"Why?\" comes before buf3\n");
else if (res == 0)
wprintf(L"buf1 and \"Why?\" are equal\n");
else
wprintf(L"buf3 comes before \"Why?\"\n");
}
Example Output
The output of this program might vary based on the LC_COLLATE category of the
current locale.