6.23.62 wmemset Function
Sets locations in an object to a specified value
Attention: This function is implemented
only by MPLAB XC32 C compilers.
Include
<wchar.h>
Prototype
wchar_t * wmemset(wchar_t * s, wchar_t c, size_t
n);
Arguments
s- the object to modify
c- the value to set
n- the number of locations to set
Return Value
A copy of s.
Remarks
The function sets the first n wide characters of the object pointed to by
s to be the value c.
Example
#include <wchar.h>
#include <stdio.h>
int main(void)
{
wchar_t ws1[20] = L"What time is it?";
wchar_t ws2[20] = L"";
wchar_t ch1 = L'?', ch2 = L'y';
wchar_t * ptr;
int res;
printf("wmemset(\"%ls\", \'%lc\',4);\n", ws1, ch1);
wmemset(ws1, ch1, 4);
printf("ws1 after wmemset: %ls\n", ws1);
printf("\n");
printf("wmemset(\"%ls\", \'%lc\',10);\n", ws2, ch2);
wmemset(ws2, ch2, 10);
printf("ws2 after wmemset: %ls\n", ws2);
}
Example Output
wmemset("What time is it?", '?',4);
ws1 after wmemset: ???? time is it?
wmemset("", 'y',10);
ws2 after wmemset: yyyyyyyyyy