6.23.40 wcsncat Function
Concatenate a wide string with another.
Include
<wchar.h>
Prototype
wchar_t * wcsncat( wchar_t * restrict s1, const wchar_t * restrict s2,
size_t n);
Arguments
s1- the wide string to append to
s2- the wide string to append
n- the maximum number of wide characters to append
Return Value
A copy of s1.
Remarks
The function appends no more than n wide characters of the wide string
pointed to by s2 to the location of the null wide character at the end of the
wide string pointed to by s1, stopping if a null wide character is
encountered. A null wide character is then appended to the end of s1,
implying that up to n+1 wide characters could be appended.
Example
#include <wchar.h>
int main(void)
{
wchar_t ws[40] = L"A long";
wcsncat(ws, L" time ago...", 5);
wprintf(L"the complete wide string is \"%ls\"\n", ws);
}
Example Output
the complete wide string is "A long time"