6.23.43 wcspbrk Function
Search a wide string for the first occurrence of a wide character from a specified set of wide characters.
Include
<wchar.h>
Prototype
wchar_t *wcspbrk(const wchar_t * s1, const wchar_t * s2);
Arguments
s1- the wide string in which to search
s2- the wide characters to search for
Return Value
Returns a pointer to the matched wide character in s1 if found; otherwise,
returns a null pointer.
Remarks
This function will search s1 for the first occurrence of a character
contained in s2.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <wchar.h>
int main(void)
{
wchar_t ws1[20] = L"What time is it?";
wchar_t ws2[20] = L"xyz";
wchar_t ws3[20] = L"eou?";
wchar_t *ptr;
int res;
wprintf(L"wcspbrk(\"%ls\", \"%ls\")\n", ws1, ws2);
ptr = wcspbrk(ws1, ws2);
if (ptr != NULL)
{
res = ptr - ws1 + 1;
wprintf(L"match found at position %d\n", res);
}
else
wprintf(L"match not found\n");
wprintf(L"\n");
wprintf(L"wcspbrk(\"%ls\", \"%ls\")\n", ws1, ws3);
ptr = wcspbrk(ws1, ws3);
if (ptr != NULL)
{
res = ptr - ws1 + 1;
wprintf(L"match found at position %d\n", res);
}
else
wprintf(L"match not found\n");
}
Example Output
wcspbrk("What time is it?", "xyz")
match not found
wcspbrk("What time is it?", "eou?")
match found at position 9