6.23.31 wcrtomb Function
Convert a wide character to a multibyte character sequence.
Include
<wchar.h>
Prototype
size_t wcrtomb(char * restrict s, wchar_t wc, mbstate_t * restrict
ps);
Arguments
s- the mulitbyte character sequence to convert
wc- a pointer to the array to hold the wide character
ps- a pointer to a
mbstate_tobject that holds the current conversion state
Return Value
The function returns the number of bytes stored in the array object s
(including any shift sequences). If wc is not a valid wide character,
(size_t)(-1) is returned.
Remarks
If s is a null pointer, the function is equivalent to the call
wcrtomb(buf, L'\0', ps), where buf represents an internal
buffer
If s is not a null pointer, the function determines the number of bytes
needed to represent the multibyte character sequence that corresponds to the wide character
given by wc (including any shift sequences), and stores at most
MB_CUR_MAX bytes of that multibyte character representation in the array
whose first element is pointed to by s. If wc is a null wide
character, a null byte is stored, preceded by any shift sequence needed to restore the initial
shift state; the resulting state described is the initial conversion state.
An encoding error occurs if wc is not a valid wide character, and the
function will store the value of the macro EILSEQ in errno
and the conversion state is unspecified.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <wchar.h>
#include <stdio.h>
#include <stdlib.h>
int main(void) {
const wchar_t * pt = L"The wide ocean";
char buffer [MB_CUR_MAX];
size_t length, i;
mbstate_t mbs;
char needNL = 0;
mbrlen (NULL, 0, &mbs); /* initialize mbs */
while (*pt) {
length = wcrtomb(buffer, *pt, &mbs);
if((length==0) || (length>MB_CUR_MAX))
break;
else
needNL = 1;
putchar ('[');
for(i=0; i<length; i++)
putchar(buffer[i]);
putchar(']');
pt++;
}
if(needNL)
putchar('\n');
}
Example Output
[T][h][e][ ][w][i][d][e][ ][o][c][e][a][n]