3.10.7 RMON History Configuration
Use this command to configure RMON history on a port.
Command Syntax:
rmon collection history <id> [ buckets <buckets> ] [ interval <interval> ]Argument | Description | |
Parameter |
| Indicates the index of the entry. The range is from 1–65535. |
| Indicates the maximum data entries associated this History control entry stored in RMON. The range is from 1–3600, the default value is 50. | |
| Indicates the interval in seconds for sampling the history statistics data. The range is from 1–3600, the default value is 1800 seconds. | |
Default | N.A | |
Mode | Port List Interface mode | |
Usage | Configure Remote Monitoring history on an interface. To delete the entry, use the ‘no’ version of the command. | |
Example | Example 1: Configure RMON history on port 2 with ID1, maximum data entries 40, and interval 1500 seconds. Example 2: Delete RMON history entry ID1. | |