3.10.20 RADIUS Server Configuration
Use this command to set default values to be used for every new RADIUS server being added when the same parameters are left blank.
Command Syntax:
radius-server timeout <seconds>
radius-server retransmit <retries>
radius-server deadtime <minutes>
radius-server key { [ unencrypted ] <unencrypted_key> | encrypted <encrypted_key> }
radius-server attribute 4 <ipv4>
radius-server attribute 95 <ipv6>
radius-server attribute 32 <id>Argument | Description | |
Parameter |
| Time to wait for a RADIUS server to reply, in seconds (1–1000), before retransmitting the request. The default value is 5. |
| The number of times a request is retransmitted to a server that is not responding, the value ranges from 1–1000. The default value is 3. | |
| Period between 0 and 1440 minutes during which the switch will not send a new request to a server that failed to respond to previous requests (dead). The default value is 0. | |
| Specify the unencrypted or encrypted key up to 63 characters long. | |
| IPv4 address to be used as attribute 4 in RADIUS Access-Request packets. If this field is left blank, the IP address of the outgoing interface is used. | |
| IPv6 address to be used as attribute 95 in RADIUS Access-Request packets. If this field is left blank, the IP address of the outgoing interface is used. | |
| The identifier - up to 253 characters long - to be used as attribute 32 in RADIUS Access-Request packets. If this field is left blank, the NAS-Identifier is not included in the packet. | |
Default | N.A | |
Mode | Global Configuration mode | |
Usage | Configure default global parameters for RADIUS Server. To revert to the default, use the ‘no’ version of the command. | |
Example | Example 1: | |
Use this command to add a new RADIUS server. Up to 5 servers can be added.
radius-server host <host_name> [ auth-port <auth_port> ] [ acct-port <acct_port> ] [ timeout <seconds> ] [ retransmit <retries> ] [ key { [ unencrypted ] <unencrypted_key> | encrypted <encrypted_key> } ]Argument | Description | |
Parameter |
| IPv4/IPv6 address or the hostname of the radius server |
| UDP port number to use on the RADIUS server for authentication. To disable authentication, set the value to 0. | |
| UDP port number to use on the RADIUS server for accounting. To disable accounting, set value to 0. | |
| Time to wait for this RADIUS server to reply (overrides default). | |
| Specify the number of retries to active server (overrides default). | |
| The unencrypted (plain text) or an encrypted secret key. | |
Default | N.A | |
Mode | Global Configuration mode | |
Usage | Configure custom parameters for RADIUS Server. To delete the server entry, use the ‘no’ version of the command. | |
Example | Example 1: | |