3.10.1 Add Local User to the Switch or Change Password
Use this command to add, remove, or change the password of local users. Up to 20 users can be configured.
Command Syntax:
username { default-administrator | <input_username> } privilege <priv> password { unencrypted <unencry_password> | encrypted <encry_password> | none }Argument | Description | |
Parameter |
| User name allows letters, numbers and underscores |
| User privilege level 0–15. Note: Use only privilege level 15. | |
| The unencrypted (plain text) user password. Any printable characters including space are accepted. Note that you have no chance to get the plain text password after this command. The system always displays the encrypted password. | |
| The encrypted (hidden) user password. Note that the encrypted password is decoded by the system internally. You cannot directly use it as same as the plain text and it is not human-readable text normally. | |
| NULL password | |
Default | N.A | |
Mode | Global Configuration mode | |
Usage | Add a new user for the local switch access and add/change password. | |
Example | Example 1: Add a user named "usertest" with unencrypted password of "testuser". Example 2: Remove user named "usertest". Example 3: Change the password of "usertest" to "testuser123". | |