3.10.6 RMON Statistics Configuration
Use this command to configure RMON Statistics on a port.
Command Syntax:
rmon collection stats <id>Argument | Description | |
Parameter |
| Indicates the index of the entry. The range is from 1 to 65535. |
Default | N.A | |
Mode | Port List Interface mode | |
Usage | Configure Remote Monitoring Collection on an interface. To disable it, use the ‘no’ version of the command. | |
Example | Example 1: Configure RMON on port 2 with ID1. Example 2: Delete RMON on port 2 with ID1. | |