3.10.13 ACL Rate Limiter Configuration
Use this command to configure the rate limiter for the ACL of the switch.
Command Syntax:
access-list rate-limiter [ <rate_limiter_list> ] { pps <pps_rate> | 100pps <pps100_rate> | 100kbps <kpbs100_rate> }Argument | Description | |
Parameter |
| The rate limiter ID. The range is 1 to 16. |
| pps rate value. The range is 0 to 99. | |
| pps rate value. The range is 0 to 10920. | |
| Kbps rate value. The range is 0 to 10000. | |
Default | N.A | |
Mode | Global Configuration mode | |
Usage | Configure the rate limiter. To disable ACL rate limiter, use the ‘no’ version of the command. | |
Example | Example 1: Configure the access list rate limiter ID1 to 300 pps. Example 2: Disable ACL rate limiter. | |