22.5 FIIC Controller Register Bit Definitions

The following tables provide the bit definitions for registers in the FIIC. 

Table 22-7. INTERRUPT_ENABLE0
Bit NumberNameReset ValueDescription
0SPIINT0_ENBL0SPIINT0 interrupt from the MSS SPI_0 block to fabric.

1: Enable

0: Mask

1SPIINT1_ENBL0SPIINT1 interrupt from the MSS SPI_1 block to fabric.

1: Enable

0: Mask

2I2C_INT0_ENBL0I2C_INT0 interrupt from the MSS I2C_0 block to fabric.

1: Enable

0: Mask

3I2C_INT1_ENBL0I2C_INT1 interrupt from the MSS I2C_1 block to fabric.

1: Enable

0: Mask

4MMUART0_INTR_ENBL0MMUART0_INTR interrupt from the MSS MMUART_0 block to fabric.

1: Enable

0: Mask

5MMUART1_INTR_ENBL0MMUART1_INTR interrupt from the MSS MMUART_1 block to fabric.

1: Enable

0: Mask

6MAC_INT_ENBL0MAC_INT interrupt from the MSS Ethernet MAC block to fabric.

1: Enable

0: Mask

7USB_MC_INT_ENBL0USB_MC_INT interrupt from the MSS USB block to fabric.

1: Enable

0: Mask

8PDMAINTERRUPT_ENBL0PDMAINTERRUPT interrupt from the MSS peripheral DMA block to fabric.

1: Enable

0: Mask

9HPD_XFR_CMP_INT_ENBL0 HPD_XFR_CMP_INT interrupt from the MSS HPDMA block to fabric.

1: Enable

0: Mask

10TIMER1_INTR_ENBL0TIMER1_INTR interrupt from the MSS TIMER1 block to fabric.

1: Enable

0: Mask

11TIMER2_INTR_ENBL0TIMER2_INTR interrupt from the MSS TIMER2 block to fabric.

1: Enable

0: Mask

12CAN_INTR_ENBL0CAN_INTR interrupt from the MSS CAN controller block to fabric.

1: Enable

0: Mask

13RTC_WAKEUP_INTR_ENBL0RTC_WAKEUP_INTR interrupt from the MSS RTC block to fabric.

1: Enable

0: Mask

14WDOGWAKEUPINT_ENBL0WDOGWAKEUPINT interrupt from the MSS Watchdog block to fabric.
  • 1: Enable
  • 0: Mask

The watchdog is refreshed by writing to the WDOGREFRESH register. When the counter value is greater than the value in the WDOGMVRP register and SLEEPING input to the watchdog is asserted, the WDOGWAKEUPINT interrupt is generated.

15MSSDDR_PLL_LOCKLOST_INT
_ENBL0MSSDDR_PLL_LOCKLOST_INT interrupt from MPLL to the fabric.

1: Enable

0: Mask

16ENVM_INT0_ENBL0ENVM_INT0 interrupt from the MSS ENVM0 block to fabric.

1: Enable

0: Mask

17ENVM_INT1_ENBL0ENVM_INT1 interrupt from MSS ENVM1 block to fabric.

1: Enable

0: Mask

18I2C_SMBALERT0_ENBL0I2C_SMBALERT0 interrupt from MSS I2C_0 block to fabric.

1: Enable

0: Mask

19I2C_SMBSUS0_ENBL0I2C_SMBSUS0 interrupt from the MSS I2C_0 block to fabric.

1: Enable

0: Mask

20I2C_SMBALERT1_ENBL0I2C_SMBALERT1 interrupt from the MSS I2C_1 block to fabric.

1: Enable

0: Mask

21I2C_SMBSUS1_ENBL0I2C_SMBSUS1 interrupt from the MSS I2C_1 block to fabric.

1: Enable

0: Mask

22HPD_XFR_ERR_INT_ENBL0HPD_XFR_ERR_INT interrupt from the MSS HPDMA block to fabric.

1: Enable

0: Mask

23MSSDDR_PLL_LOCK_INT_ENBL0MSSDDR_PLL_LOCK_INT interrupt from the MPLL block to fabric.

1: Enable

0: Mask

24SW_ERRORINTERRUPT_ENBL0SW_ERRORINTERRUPT interrupt from the SYSREG block to fabric.

1: Enable

0: Mask

HRESP from AHB bus Matrix assertion to the master in case of blocked fabric master or for the unimplemented address space results in SW_ERRORINTERRUPT signal.

In case of above error condition the following signals are ORed together in SYSREG to create the SW_ERRORINTERRUPT signal:

1. HRESP assertion being issued to the HPDMA.

2. HRESP assertion being issued to FIC_0.

3. HRESP assertion being issued to FIC_1.

4. HRESP assertion being issued to the Ethernet MAC.

5. HRESP assertion being issued to the peripheral DMA engine.

6. HRESP assertion being issued to the USB.

7. HRESP assertion being issued to the system controller.

25DDRB_INTR_ENBL0MSS DDR bridge DDRB_INTR to fabric.

1: Enable

0: Mask

DDRB_INTR input indicates that any one of the following interrupts are asserted from the MSS DDR bridge:

DDRB_ERROR interrupts

DDRB_DISABLEDONE interrupts

DDRB_LOCKTIMEOUT interrupts

26ECCINTR_ENBL0ECCINTR interrupt from ESRAM0, ESRAM1 CAN, MDDR, and USB to fabric.
  • 1: Enable
  • 0: Mask

The ECCINTR interrupt is asserted when an SECDED error has been detected in ESRAM0, ESRAM1, CAN, MDDR, or USB memories.

27CACHE_ERRINTR_ENBL0CACHE_ERRINTR interrupt from the cache controller block to fabric.

1: Enable

0: Mask

The CACHE_ERRINTR interrupt is generated in the SYSREG block by ORing of the following interrupts from the SmartFusion 2 SoC FPGA CACHE block:

CC_HRESPERRINT0

CC_HRESPERRINT1

CC_HRESPERRINT2

CC_HRESPERRINT3

CC_EDCERRINT

28SOFTINTERRUPT_ENBL0SOFTINTERRUPT interrupt from the SYSREG block to fabric.

1: Enable

0: Mask

SOFTINTERRUPT is set by the Cortex-M3 processor firmware by writing to the soft interrupt SYSREG block bits.

29COMBLK_INTR_ENBL0COMBLK_INTR interrupt from the COMM_BLK block to fabric.

1: Enable

0: Mask

30USB_DMA_INT_ENBL0USB_DMA_INT interrupt from USB’s DMA controller to fabric.

1: Enable

0: Mask

31Reserved0Reserved

 

Table 22-8. INTERRUPT_ENABLE1
Bit NumberNameReset ValueDescription
0Reserved0Reserved
1Reserved0Reserved
2Reserved0Reserved
3MDDR_IO_CALIB_INT_ENBL0MDDR_IO_CALIB_INT interrupt from the MDDR block to fabric.

1: Enable

0: Mask

4Reserved0Reserved
5FAB_PLL_LOCK_INT_ENBL0FAB_PLL_LOCK_INT interrupt from FAB_PLL.

1: Enable

0: Mask

6FAB_PLL_LOCKLOST_INT_ENBL0FAB_PLL_LOCKLOST_INT interrupt from FAB_PLL.

1: Enable

0: Mask

7FIC64_INT_ENBL0FIC64_INT interrupt from the DDR_FIC block.

1: Enable

0: Mask

8-31Reserved0Reserved

 

Table 22-9. INTERRUPT_REASON1
Bit NumberNameReset ValueDescription
0Reserved0Reserved
1Reserved0Reserved
2Reserved0Reserved
3MDDR_IO_CALIB_INT_STATUS0Set if the interrupt source for MDDR_IO_CALIB_INT is asserted and the MDDR_IO_CALIB_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE1 is High.
4Reserved0Reserved
5FAB_PLL_LOCK_INT_STATUS0Set if the interrupt source for FAB_PLL_LOCK_INT is asserted and the FAB_PLL_LOCK_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE1 is High.
6FAB_PLL_LOCKLOST_INT_STATUS0Set if the interrupt source for FAB_PLL_LOCKLOST_INT is asserted and the FAB_PLL_LOCKLOST_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE1 is High.
7FIC64_INT_STATUS0Set if the interrupt source for FIC64_INT is asserted and the FIC64_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE1 is High.
8-31Reserved0Reserved

 

Table 22-10. INTERRUPT_REASON0
Bit NumberNameReset ValueDescription
0SPIINT0_STATUS0Set if the interrupt source for SPIINT0 is asserted and the SPIINT0_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
1SPIINT1_STATUS0Set if the interrupt source for SPIINT1 is asserted and the SPIINT1_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
2I2C_INT0_STATUS0Set if the interrupt source for I2C_INT0 is asserted and the I2C_INT0_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
3I2C_INT1_STATUS0Set if the interrupt source forI2C_INT1 is asserted and the I2C_INT1_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
4MMUART0_INTR_STATUS0Set if the interrupt source for MMUART0_INTR is asserted and the MMUART0_INTR_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
5MMUART1_INTR_STATUS0Set if the interrupt source for MMUART1_INTR is asserted and the MMUART1_INTR_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
6MAC_INT_STATUS0Set if the interrupt source for MAC_INT is asserted and the MAC_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
7USB_MC_INT_STATUS0Set if the interrupt source for USB_MC_INT is asserted and the USB_MC_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
8PDMAINTERRUPT_STATUS0Set if the interrupt source for PDMAINTERRUPT is asserted and the PDMAINTERRUPT_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
9HPD_XFR_CMP_INT_STATUS0Set if the interrupt source for HPD_XFR_CMP_INT is asserted and the HPD_XFR_CMP_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
10TIMER1_INTR_STATUS0Set if the interrupt source for TIMER1_INTR is asserted and the TIMER1_INTR_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
11TIMER2_INTR_STATUS0Set if the interrupt source for TIMER2_INTR is asserted and the TIMER2_INTR_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
12CAN_INTR_STATUS0Set if the interrupt source for CAN_INTR is asserted and the CAN_INTR_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
13RTC_WAKEUP_INTR_STATUS0Set if the interrupt source for RTC_WAKEUP_INTR is asserted and the RTC_WAKEUP_INTR_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
14WDOGWAKEUPINT_STATUS0Set if the interrupt source for WDOGWAKEUPINT is asserted and the WDOGWAKEUPINT_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
15MSSDDR_PLL_LOCKLOST_INT_STATUS0Set if the interrupt source for MSSDDR_PLL_LOCKLOST_INT is asserted and the MSSDDR_PLL_LOCKLOST_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
16ENVM_INT0_STATUS0Set if the interrupt source for ENVM_INT0 is asserted and the ENVM_INT0_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
17ENVM_INT1_STATUS0Set if the interrupt source for ENVM_INT1 is asserted and the ENVM_INT1_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
18I2C_SMBALERT0_STATUS0Set if the interrupt source for I2C_SMBALERT0 is asserted and the I2C_SMBALERT0_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
19I2C_SMBSUS0_STATUS0Set if the interrupt source for I2C_SMBSUS0 is asserted and the I2C_SMBSUS0_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
20I2C_SMBALERT1_STATUS0Set if the interrupt source for I2C_SMBALERT1 is asserted and the I2C_SMBALERT1_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
21I2C_SMBSUS1_STATUS0Set if the interrupt source for I2C_SMBSUS1 is asserted and the I2C_SMBSUS1_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
22HPD_XFR_ERR_INT_STATUS0Set if the interrupt source for HPD_XFR_ERR_INT is asserted and the HPD_XFR_ERR_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
23MSSDDR_PLL_LOCK_INT_STATUS0Set if the interrupt source for MSSDDR_PLL_LOCK_INT is asserted and the MSSDDR_PLL_LOCK_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.

MSSDDR_PLL_LOCK_INT interrupt is asserted when MPLL achieves lock.

24SW_ERRORINTERRUPT_STATUS0Set if the interrupt source for SW_ERRORINTERRUPT is asserted and the SW_ERRORINTERRUPT_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
25DDRB_INTR_STATUS0Set if the interrupt source for DDRB_INTR is asserted and the DDRB_INTR_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
26ECCINTR_STATUS0Set if the interrupt source for ECCINTR is asserted and the ECCINTR_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
27CACHE_ERRINTR_STATUS0Set if the interrupt source for CACHE_ERRINTR is asserted and the CACHE_ERRINTR_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
28SOFTINTERRUPT_STATUS0Set if the interrupt source for SOFTINTERRUPT is asserted and the SOFTINTERRUPT_ENBL interrupt enable bit inINTERRUPT_ENABLE0 is High.
29COMBLK_INTR_STATUS0Set if the interrupt source for COMBLK_INTR is asserted and the COMBLK_INTR_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
30USB_DMA_INT_STATUS0Set if the interrupt source for USB_DMA_INT is asserted and USB_DMA_INT_ENBL interrupt enable bit in INTERRUPT_ENABLE0 is High.
31Reserved0Reserved
Table 22-11. INTERRUPT_MODE
Bit NumberNameReset ValueDescription
0SELECT_MODE0The following are the valid values for this bit:

0: Select group 0

1: Select group 1

31:1Reserved0Reserved