28.2.5 __builtin_clr
Description
Clear the specified accumulator.
For example:
volatile register int32_t result asm("A");
result = __builtin_clr();
will generate:
clr A
Prototype:
int32_t __builtin_clr(void);
Argument
None
Return Value
Returns the cleared value result to an accumulator.
Assembler Operator/ Machine Instruction
clr a
Error Messages
An error message will be displayed if the result is not an accumulator register.