1.3.5.6.59 BMNG_PPROF_ResetRequest Function
C
void BMNG_PPROF_ResetRequest(uint8_t cmd, uint8_t *eui48);
Summary
Requests to reset all PIB statistics attributes of a node using the PRIME Profile.
Description
This routine requests to reset all PIB statistics attributes of a node using the PRIME Profile.
Precondition
None.
Parameters
| Param | Description |
|---|---|
| cmd | Command to acknowledge |
| eui48 | Pointer to the address of the node to be reset |
Returns
None.
Example
uint8_t eui48[6];
memset(eui48, 0x12, 6);
BMNG_PPROF_ResetRequest(PPROF_RESET_REQUEST, eui48);
Remarks
The command is acknowledged with the PPROF ACK callback.