1.3.5.6.11 BMNG_FUP_ABORT_FU_REQUEST Function Pointer
C
typedef void (*BMNG_FUP_ABORT_FU_REQUEST)(uint8_t cmd, uint8_t *eui48);
Summary
Function pointer to request to abort an ongoing firmware upgrade process.
Description
This data type contains the definition of the function pointer to abort an ongoing firmware upgrade process.
- cmd: Command to acknowledge
- eui48: Pointer to the address of the node to be aborted
Remarks
If the MAC address is FF:FF:FF:FF:FF:FF, the FU is aborted for all nodes.
The command is acknowledged with the FUP ACK callback.