1.3.5.6.52 BMNG_FUP_AbortFuRequest Function
C
void BMNG_FUP_AbortFuRequest(uint8_t cmd, uint8_t *eui48);
Summary
Requests to abort an ongoing firmware upgrade process.
Description
This routine requests to abort an ongoing firmware upgrade process.
Precondition
The firmware upgrade process must have been started before.
Parameters
| Param | Description |
|---|---|
| cmd | Command to acknowledge |
| eui48 | Pointer to the address of the node to be aborted |
Returns
None.
Example
uint8_t eui48[6];
memset(eui48, 0x12, 6);
BMNG_FUP_AbortFuRequest(FUP_CLEAR_ADD_TARGET_REQUEST, eui48);
Remarks
If the MAC address is FF:FF:FF:FF:FF:FF, the FU is aborted for all nodes.
The command is acknowledged with the FUP ACK callback.