2.76.1 PDECx_QDECInitialize Function
C
void PDECx_QDECInitialize ( void ); // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Initializes given instance of PDEC peripheral in quadrature mode.
Description
This function initializes given instance of PDEC peripheral in quadrature mode with options configured in MCC GUI.
Precondition
MCC GUI should be configured with the desired options.
Parameters
None.
Returns
None.
Example
PDEC_QDECInitialize();
Remarks
This function must be called before any other PDEC function is called. This function is normally called only be called once during system initialization.