2.76.12 PDECx_HALLPatternGet Function

C

uint8_t PDECx_HALLPatternGet ( void ) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.

Summary

Reads the hall pattern.

Description

This function reads the hall pattern tracked by the channel counter COUNT LSB.

Precondition

PDECx_HALLInitialize function must have been called first for the given channel.

Parameters

None.

Returns

Returns the hall pattern.

Example

uint8_t position;

PDEC_HALLInitialize();
PDEC_HALLStart();
position = PDEC_HALLPositionGet();

Remarks

None