2.76.4 PDECx_QDECPositionGet Function
C
uint16_t PDECx_QDECPositionGet ( void ) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.
Summary
Reads the angular position from the quadrature encoder.
Description
This function reads the position from the quadrature encoder by reading as tracked by the channel counter.
Precondition
PDECx_QDECInitialize function must have been called first for the given channel.
Parameters
None.
Returns
Returns Position of the encoder. This consists of the angular position and revolution counter.
Example
int16_t position; PDEC_QDECInitialize(); PDEC_QDECStart(); position = PDEC_QDECPositionGet();
Remarks
In counter-clockwise direction, position counter works in down counting mode. Returned position must be decoded as angular position and revolution counter based on the ANGULAR bit field value.