2.59.4 LEDx_DutyCycleMaxSet Function

C

/* x = LED peripheral instance number */

void LEDx_DutyCycleMaxSet(uint8_t max)

Summary

Specifies the maximum duty cycle value.

Description

when the current duty cycle is greater than or equal to the max value the breathing apparatus holds the current duty cycle for the period specified by the field HD in register LED_DELAY

Precondition

None

Parameters

ParamDescription
maxMaximum value of the duty cycle in LED breathing mode

Returns

None

Example

LED0_DutyCycleMaxSet(200);

Remarks

None