2.99.17 SDHCx_ModuleInit Function

C

/* x = SDHC instance number (x is applicable only on devices with more than one instances of SDHC) */

void SDHCx_ModuleInit ( void )

Summary

Initializes the SDHC peripheral.

Description

This function initializes the SDHC peripheral. The SDHC peripheral is initialized in 1 bit mode and the SDHC clock is set to 400 kHz. This function may be called at run time to re-initialize the peripheral to the initial state.

Precondition

None.

Parameters

None.

Returns

None.

Example

SDHC1_ModuleInit();

Remarks

None.