15.3.23 Cross-probing Between NetlistViewer and SmartTime
Use NetlistViewer with SmartTime to view and trace entire Timing paths and to cross-probe one or more objects.
Note: Your design must be compiled to start NetlistViewer. If it is
not compiled, Designer prompts you to compile your design. After you compile it,
NetlistViewer opens and displays the netlist.
To cross-probe an object using NetlistViewer and SmartTime:
In the Design Flow window,
click NetlistViewer to display your netlist, and then click
Timing Analyzer to display the SmartTime
Timing Analyzer.
In the SmartTimeTiming
Analyzer, select the clock domain in the Domain
Browser.
Select a path in the Paths List, right-click it, and choose
Expand selected paths from the right-click menu.
Select any instance in the
SmartTime Expanded Path View. The instance appears
highlighted in both SmartTime and NetlistViewer as shown in the following
example.
To select multiple instances, hold down the Shift key as you click
each instance.
Figure 15-31. Selected Instance Appears Highlighted in Both SmartTime and
NetlistViewer
To cross-probe a path, right-click
the path, and choose Cross-probe Path from the right-click
menu (as shown in the following example).Figure 15-32. Cross-probe Path Using Right-click Menu
All objects in the selected path appear highlighted in NetlistViewer as shown below.Figure 15-33. All Objects in the Cross-probed Path Appear Highlighted in
NetlistViewer
Changing the highlight color does not change the color of all cross-probed paths in
NetlistViewer. To change the color of a cross-probed path, from the Edit menu, choose
Highlight Color and select a different color. Then cross-probe the path again in
SmartTime. The cross-probed path will appear in the new highlight color.
For more information, see the SmartTime User’s Guide.