15.3.9 Changing the Name of a Cone

You can modify the name of any Logical Cone view. The new name appears in the title bar of the cone window as well as in the Logical Cones tab of the Hierarchy window.

To change the name of a cone:

  1. Select a Logical Cone view.
  2. From the LogicalCone menu, choose Rename Cone.
  3. In the Rename Cone dialog box, type the new name over the existing one.
  4. Click OK.
Note:
  • The Rename Cone command is available only when the current window is a Logical Cone view.
  • You can also rename a cone from the Logical Cones tab in the Hierarchy window. Click once on the cone name to select it, and click again to edit it. When you see an outline around the highlighted name, type the new name in place of the old one.