15.14.5 Logic Menu

This menu is available only for the ChipPlanner, PinEditor, and I/O Attribute Editor tools in the MultiView Navigator.

CommandIconShortcutFunction

Assign To Location

???

CTRL + K

Assigns the selected object to the selected location

Unassign From Location

???

CTRL + SHIFT + K

Unassigns the selected object from its current location

Unassign All From Location

Unassigns all instances from their location

Lock

???

CTRL + L

Locks the selected instance

Unlock

???

CTRL + SHIFT + L

Unlocks the selected locked instance

Lock All

Locks all I/Os in PinEditor or all instances in ChipPlanner

Unlock All

Unlocks all I/Os in PinEditor or all instances in ChipPlanner

Assign To Region

???

CTRL + N

Assigns the selected I/O or instance to the selected region

Unassign From Region

???

CTRL + SHIFT + N

Unassigns the selected I/O or instance from its current region

Unassign All From Region

Unassigns all I/Os and instances from the selected region

Properties

Displays the Logic Properties dialog box, in which you can change the properties of the selected logic