15.14.13 Window Menu
This menu is available for all tools in the MultiView Navigator.
| Command | Function |
|---|---|
| Close Window | Closes the currently active tool window within the Tools window If the tool has more than one window open, this command closes all the windows for that tool. |
| Cascade | Arranges windows so you can see the title bar of each window |
| Tile Horizontally | Arranges windows side-by-side in a horizontal pattern |
| Tile Vertically | Arranges windows side-by-side in a vertical pattern |
| Arrange Icons | Arranges minimized windows left-to-right across the bottom of the Tool window |
| <Tool name> | Makes the selected tool active |