15.14.4 View Menu
This menu is available for all tools in the MultiView Navigator.
| Command | Icon | Shortcut | Function |
|---|---|---|---|
|
Zoom In |
|
CTRL + + |
Magnifies the view by a factor of 2 (scale = 2x) If using the keyboard shortcut, use the + on the numeric keypad only. |
|
Zoom Out |
|
CTRL + - |
Reduces the view by a factor of 2 (scale = .5x) If using the keyboard shortcut, use the - on the numeric keypad only. |
|
Zoom Window |
|
CTRL + W |
Drag out an area to enlarge |
|
Zoom Fit |
|
CTRL + 0 |
Fits the entire design within the active Tools window |
|
Redraw |
Redraws the screen | ||
|
Active List |
Displays a submenu of choices: <User-defined lists> - displays user-defined lists <Pre-defined lists> - displays any pre-defined lists such as Unassigned Macros, Unassigned I/Os, etc. Edit Current Active List - displays the Edit Active List dialog box with the settings for the current Active List. More Lists - displays a dialog box in which you can choose to create a new list, edit a list, copy a list, or delete a list. | ||
|
Toolbars |
Hides or displays groups of toolbar buttons | ||
|
Windows |
Hides or displays the Hierarchy window, Log window, Status Bar, or World window | ||
|
Display Settings |
CTRL + D |
Displays the Display Settings dialog box, which provides a list of all the architectural features you can turn on and off in your tool | |
|
Properties |
Displays the ChipPlanner Properties dialog box, which enables you tochoosewhether you want to bring a macro or net into view after you select it |