15.14.10 LogicalCone Menu

This menu is available only for the NetlistViewer tool and Logical Cone windows in the MultiView Navigator.

CommandShortcutFunction

Create New Cone

Opens a new Logical Cone window, which is set as the active cone

Rename Cone

Displays a dialog box, in which you can change the name of the active cone

Fold Selection

Hides all the logic inside the selected hierarchical instance in the cone view

Unfold Selection

Shows the logic that was added into the selected hierarchical instance in the cone view

Add to Active Cone

Displays a submenu of choices:
  • Selection - adds selected objects to the active cone
  • Highlighted Group - adds a group of highlighted objects to the active cone
  • Driver - adds the instances which have a pin driving the selected net, input pin, or instance to the active cone
  • All Driven Logic - adds all instances which have a pin driven by the selected net, output pin, or instance to the active cone
  • Adjacent Logic- displays a dialog box in which you select instances to add to the active cone

Remove From Active Cone

Displays a submenu of choices:
  • All Logic - removes all objects from the active cone
  • Selection - removes the selected object from the active cone
  • Highlighted Group - removes the selected group of objects from the active cone