21.15.2 SDC Syntax Conventions

The following table shows the typographical conventions that are used for the SDC command syntax.

Table 21-54. Typographical Conventions
Syntax NotationDescription

command - argument

Commands and arguments appear in Courier New typeface.

variable

Variables appear in blue, italic Courier New typeface. You must substitute an appropriate value for the variable.

[-argument

value]

Optional arguments begin and end with a square bracket.

Note: SDC commands and arguments are case sensitive.