10.2.1 Fusion Dynamic CCC
Fusion Dynamic CCC is a clock conditioning core that enables dynamic reconfiguration of the PLL through a serial shift-register interface.
Related Topics
Key Features
The only difference between the Fusion Dynamic CCC and Fusion Static PLL is the availability of the dynamic shift register signals that enable a dynamic reconfiguration of the PLL. The Dynamic CCC (clock conditioning core) enables you to change the CCC configuration by shifting it in through a serial interface. You have a fixed default configuration and the two configurations can be interchanged dynamically.
The Dynamic CCC for Fusion contains a PLL core, delay lines, clock multipliers/dividers, PLL reset generator (you have no control over the reset), global pads and all circuitry for the selection and interconnection of the “global” pads to the global network. The PLL Core consists of a Phase Detector, L.P. Filter and a 4-phase VCO along with the following:
- RC Oscillator Clock Source – If you choose RC Oscillator as the clock source the input frequency is fixed at 100 MHz. The divide-by-half feature is available if you bypass the PLL for the primary output.
- Divide-by-half behavior – Available if clock source is RC Oscillator and PLL is bypassed for the given output (A, B, C). When activated, the output divider (U, V or W) gets divided by 2.
- Crystal oscillator clock source – No special configuration options are available if you use the crystal oscillator as your clock source.
- Availability of output dividers in bypass mode – If you bypass the PLL in the primary output, you can specify an output frequency that is some divisible of the input frequency.
The Static PLL performs the following basic functions:
- Clock phase adjustment
- Clock delay minimization
- Clock frequency synthesis
In addition it also performs the following functions:
- Enables access from the global pads to the global network and the PLL block
- Permits the three global lines on each side of the chip to be driven either by the global pads, core and/or the outputs from the PLL block
- Enables access from PLL to the core
The block contains several programmable dividers, each of them providing division factors 1, 2, 3, 4 … k (where k depends on the number of bits used for the division selection).
m/(n * u)
m/(n * v)
m/(n * w)
The clock conditioning circuit block performs a positive/negative clock delay operation in increments of 200 ps, of up to 6.735 ns (at 1.5 V, 25 °C, typical process).
Furthermore, the system allows for the selection of one of four clock phases of fout, at 0, 90, 180 and 270 degrees.
A “Lock” signal is provided to indicate that the PLL has locked on to the incoming signal. A “Power-down” signal switches off the PLL block when it is not used.