15.7.14.2 Prelayout Physical Constraint Verification
The prelayout checker performs the following DRC (Design Rule Checker) checks:
- The remaining clocks, which need to be assigned
to a global clock resource, need to be less than 6. For
example:
Resource Limit The number of chip globals in your design exceeded the maximum number available in the device. - The checker verifies that the total
number of clock resources assigned to the given quadrant does not exceed 3. For
example:
PRL09: The number of clocks assigned (4) to the Upper Left quadrant exceeds the maximum number available (3) in the device. - If a clock is placed and assigned to
a quadrant clock region, the checker verifies that the clock is placed in the given
quadrant clock region. For
example:
PRL11: Cannot assign net:net_out2 to the Upper Right quadrant and its driver macro:clkbibuf1 to Upper Left quadrant which is outside the quadrant.