9.7.11 Reuse Serial Data
If a device fails to program and the Reuse Serial Data serialization setting is selected, the software automatically reuses the current serial data when programming the next device.
Note: The default FlashPro serialization setting is Skip Serial Data.
You can change the serialization setting in either of the following ways:
- From the Tools menu, choose Serialization.
- Click the Skip serial data icon or the Reuse Serial Data icon on the toolbar.