9.7.10 Skip Serial Data
If a programming action cannot be performed on a device, or if the device fails to program and the Skip Serial Data serialization setting is selected, the software automatically uses the next serial data when programming the next device.
Note: By default, FlashPro® is configured to use the Skip Serial
Data setting.
You can change the serialization setting in either of the following ways:
- From the Tools menu, choose Serialization.
- Click the Skip serial data icon or the Reuse Serial Data icon on the toolbar.