The Chain Configuration window displays the chain order, the chain editing
options, and the chain configuration grid. The Chain Configuration Grid
enables you to view and set options for each of your devices. Right-click a column heading in
the grid and choose a menu option to show or hide a specific column.
The Chain Configuration Grid enables you to view, sort and/or set the following options:
Device: Device name.
Name: Editable field for a user-specified device name. If you have two or more identical
devices in your chain you can use this column to give them unique names.
File: Path to programming file.
IR Length: Device instruction
length.
Max TCK (MHz):: Maximum clock frequency to program a specific device. FlashPro® uses this information to ensure that the programmer operates at a
frequency lower than the slowest device in the chain.
Enable Device: Select to enable the
device for programming.
Enable Serial: Select to enable
serialization when you have loaded a serialization programming file
Action: List of programming actions for
your device.
Procedures: Advanced option; enables you to customize the list of recommended and
optional procedures for the selected Action.
Serial Data: Opens the Serial Settings
dialog box; enables you to set your serialization data.
Serial Status: Displays serialization status; lists serialization index(es)/action(s)
that have been used and shows the next serialization data that will be programmed.
HIGH-Z - Sets disabled Actel, IGLOO®, ProASIC3, SmartFusion®, Fusion and ProASICPLUS devices in the chain to HIGH-Z
(tri-states all the I/Os) during chain programming of enabled Actel devices in the daisy
chain.
The Show Chain Editing checkbox, when checked displays your chain editing
options (Configure device, Add Actel Device, Add Non-Actel Device, and organization buttons to
move your device within the grid). For information on how to Add Actel and Non-Actel devices,
see the Chain Editing section.
Note: Note: For information on how to use the Organize buttons (located next to the Add Actel
and Add Non-Actel buttons) in the Chain Configuration grid, see the Using the Organize buttons in the Chain Programming grid section.
You can enable programming and serialization by checking the Enable Device
checkbox and the Enable Serial checkbox in the Chain
Configuration grid.Figure 9-104. Chain Configuration Window