9.7.12 Serialization with Parallel Programming
When programming the multiple ProASIC3 devices in parallel, while performing serialization at the same time, each target device is assigned a Serial Index/Action for each programming run. Upon each successful completion of each programming run, a new index is assigned to the each target device for the next programming run. This process continues until the selected Serial Indices/Actions are exhausted.
Note: If programming failure is encountered, depending on the user setting, the failed serial
data may be reused or skipped in the next programming run. If, in the last programming run,
the remaining number selected Serial Indices/Actions is less than the
number of targeted ProASIC3 devices, the targeted devices without an assigned
Serial Index/Action are skipped in the final serial programming
run.