13.29.17 Report types
You can generate the following types of reports in Designer:
| Report Type | Report | Supported Families | Report Contents | |
| Status | Status | All | Provides information about Designer, Device Data, and variable settings for the design. | |
| Timing | Timer (using SmartTime) | IGLOO, ProASIC3,SmartFusion, Fusion, Axcelerator, RTAX-S, eX, and SX-A | Provides a text report with the timing information organized by clock domain as in the GUI. | |
| Timer (using Timer) | SX, MX, 3200DX, ACT3, ACT2,and ACT1 | Displays summarized timing delays for paths. | ||
| Bottleneck | IGLOO, ProASIC3,SmartFusion, Fusion, Axcelerator, RTAX-S, eX,and SX-A | Creates a report containing information about the bottlenecks in the design. | ||
| Constraints Coverage | IGLOO, ProASIC3,SmartFusion, Fusion, Axcelerator, RTAX-S, eX, and SX-A | Creates a report containing information about the constraints in the design. | ||
| Datasheet | IGLOO, ProASIC3,SmartFusion, Fusion, Axcelerator, RTAX-S, eX, and SX-A | Creates a report containing information about the external characteristics of the design. | ||
| Timing Violations (using SmartTime) | IGLOO, ProASIC3,SmartFusion, Fusion, Axcelerator, RTAX-S, eX, and SX-A | Provides a flat slack report centered around constraint violations. | ||
| Combinational Loops | IGLOO, ProASIC3,SmartFusion, Fusion, Axcelerator, RTAX-S, eX, and SX-A | This report displays all loops found during initialization and reports pins associated with the loop(s), and the location where the loop is broken. | ||
| Resources | Pin | All | Creates a text list of the I/O signal locations on a device. You can generate a pin report sorted by I/O signal names or by package number. | |
| Flip Flop | All | Creates a report that lists the number and type of flip-flops
(sequential or CC, which are flip-flops made of 2 combinatorial macros)
used in a design. The flip-flop report can be of two types: Summary or
Extended. Both types of reports include the Flip-Flop type, sequential (Seq) or combinatorial (CC), the Library name, and the Total number of Seq and CC Flip-Flops in the design. The Summary Report also includes the Number of instances of each unique type. The Extended Report provides the Macro name. All Reports are output to an editable window for viewing, modifying, saving, and printing. | ||
| IOBank | IO Bank | IGLOO, ProASIC3,SmartFusion, Fusion, and Axcelerator | Provides information on the I/O functionality, I/O technologies, I/O banks and I/O voltages. | |
| Power | Power | IGLOO, ProASIC3,SmartFusion, Fusion, ProASICPLUS, ProASIC, and Axcelerator | Enables you to quickly determine if any power consumption problems exist in your design. The power report lists the following information: - Global device information and SmartPower Preferences selection information - Design level static power summary - Dynamic power summary - Hierarchical detailed power report (including gates, blocks, and nets), with a block by block, gate by gate, and net by net power summary SmartPower results. | |
| Power Cycle Accurate | IGLOO, ProASIC3,SmartFusion, Fusion, ProASICPLUS, ProASIC, Axcelerator, and RTAX-S | Creates a report containing a power waveform with one power value per clock period of half-period instead of an average power for the whole simulation. | ||
| Power Activity and Hazards | IGLOO, ProASIC3,SmartFusion, Fusion, ProASICPLUS, ProASIC, Axcelerator, and RTAX-S | Creates a report containing information about transitions and hazards for each clock cycle of the VCD file. | ||
| Power Scenario | IGLOO, ProASIC3,SmartFusion, Fusion, ProASICPLUS, ProASIC, Axcelerator, and RTAX-S | Creates a report containing information about the average power consumption and battery life for a sequence of previously defined operating modes. | ||
| Global | CCC Configuration | IGLOO, ProASIC3, SmartFusion and Fusion | The Fusion Dynamic CCC (DYNCCC) and ProASIC3E Dynamic CCC prints out all the values of the configuration pins in a report. You can use these to specify the bitstream that can be shifted in via the shift register. | |
| GlobalNet | ProASICPLUS, ProASIC | Creates a report containing information about the net(s) that are assigned or routed using Global or LocalClock resources. | ||
| Global Usage | ProASICPLUS, and ProASIC | Provides information about the net(s) that are assigned or routed using Global or LocalClock resources. | ||
| Block | Block Report | IGLOO, ProASIC3,SmartFusion, Fusion, Axcelerator, and RTAX-S | Creates a report specifically for Blocks and their implementation. Includes Compile, Datasheet, Global, and Interface information. | |