16.7 Using NetlistViewer (non-MVN) with ChipEditor

If both NetlistViewer and ChipEditor are open, selecting items in either tool automatically selects them in the other.

To use NetlistViewer with ChipEditor, perform the following steps:
  1. Click NetlistViewer in Designer’s Design Flow window. NetlistViewer starts and displays the netlist.
  2. Start ChipEditor. ChipEditor opens in a separate window and displays the logic and I/O modules on the device. The following figure shows the ChipEditor window.
    Figure 16-11. ChipEditor Window
  3. Selecting a macro or instance in ChipEditor automatically selects it in NetlistViewer too. Likewise, selecting a macro or instance in NetlistViewer also selects it in ChipEditor.
    Figure 16-12. Item Selected in NetlistViewer
    Figure 16-13. NetlistViewer Selected Item in ChipEditor

For more information about ChipEditor, see the ChipEditor online help or ChipEditor User Guide.