16.4 Selecting Objects

To manage object selection in NetlistViewer, use the following methods:

  • First, select an object before highlighting it. To select an object, left-click it.
  • To select multiple objects in NetlistViewer, press and hold SHIFT, and then click each object.
  • To unselect specific selected objects, press and hold SHIFT, and then click each selected object to unselect it. Also click and drag a rectangle toward the bottom-right corner; release the mouse button when all items which needs to be unselected are included in the rectangle.
  • To unselect all selected objects, click a clear spot in the Schematic window.