13.5.4.1 DO File

  • Use automatic DO file - Select if you want the Project Manager to automatically create a DO file that will enable you to simulate your design.
  • User defined DO file - Enter the DO file name or click the browse button to navigate to it.
  • Simulation Run Time - Specify how long the simulation should run. If the value is 0, or if the field is empty, there will not be a run command included in the run.do file.
  • Testbench module/entity name - Specify the name of your testbench entity name. Default is “testbench,” the value used by WaveFormer Pro.
  • Top Level instance name in the testbench - Default is <top_0>, the value used by WaveFormer Pro. The Project Manager replaces <top> with the actual top level macro when you run ModelSim.
  • DO command parameters - Text in this field is added to the DO command.
  • Generate VCD file - Click the checkbox to generate a VCD file.
  • VCD file name - Specifies the name of your generated VCD file. The default is power.vcd; click power.vcd and type to change the name.