1.1.2.4.9 DRV_G3_MACRT_TxCfmCallbackRegister Function
C
void DRV_G3_MACRT_TxCfmCallbackRegister (
const DRV_HANDLE handle,
const DRV_G3_MACRT_TX_CFM_CALLBACK callback
);
Summary
Allows a client to set a G3 MAC RT data confirm event handling function for the driver to call back when the requested transmission has finished.
Description
This function allows a client to register a G3 MAC RT data confirm event handling function for the driver to call back when a data confirmation PLC event occurs.
The event handler should be set before the client submits any transmission requests that could generate events. The callback once set, persists until the client closes the driver or sets another callback (which could be a NULL pointer to indicate no callback).
Precondition
DRV_G3_MACRT_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid instance handle, returned from the driver's open routine. |
| callback | Pointer to the callback function. |
Returns
None.
Example
// Event is received when the transmission is finished void APP_PLC_Tx_Cfm_callback(MAC_RT_TX_CFM_OBJ *cfmObj) { if (cfmObj->result == MAC_RT_STATUS_SUCCESS) { // This means the data was transferred successfully. } else { // Error handling here. } } // myAppObj is an application specific state data object. MY_APP_OBJ myAppObj; // Client registers a TX confirm callback with driver. This is done once // 'myHandle', returned from DRV_G3_MACRT_Open previously called DRV_G3_MACRT_TxCfmCallbackRegister( myAppObj.myHandle, APP_PLC_Tx_Cfm_callback ); DRV_G3_MACRT_TxRequest(myAppObj.myHandle, myAppObj.pData, myAppObj.dataLength);
Remarks
None.