1.1.2.4.11 DRV_G3_MACRT_RxParamsIndCallbackRegister Function
C
void DRV_G3_MACRT_RxParamsIndCallbackRegister (
const DRV_HANDLE handle,
const DRV_G3_MACRT_RX_PARAMS_IND_CALLBACK callback
);
Summary
Allows a client to set a G3 MAC RT reception parameters event handling function for the driver to call back when a packet reception has finished.
Description
This function allows a client to register a G3 MAC RT Rx parameters indication event handling function for the driver to call back when a new data message is received.
This callback has to be set to get the reception parameters related to a received frame, otherwise such information will be unknown. The callback once set, persists until the client closes the driver or sets another callback (which could be a NULL pointer to indicate no callback).
Precondition
DRV_G3_MACRT_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid instance handle, returned from the driver's open routine. |
| callback | Pointer to the callback function. |
Returns
None.
Example
void APP_PLC_Params_Ind_callback(MAC_RT_RX_PARAMETERS_OBJ *pParameters) { // Rx Parameters handling here. } // myAppObj is an application specific state data object. MY_APP_OBJ myAppObj; // Client registers a RxParams indication callback with driver. This is done once // 'myHandle', returned from DRV_G3_MACRT_Open previously called DRV_G3_MACRT_RxParamsIndCallbackRegister( myAppObj.myHandle, APP_PLC_Params_Ind_callback );
Remarks
None.