1.1.2.4.3 DRV_G3_MACRT_Close Function
C
void DRV_G3_MACRT_Close(const DRV_HANDLE handle);
Summary
Closes an opened instance of the G3 MAC RT driver.
Description
This routine closes an opened instance of the G3 MAC RT driver, invalidating the handle. A new handle must be obtained by calling DRV_G3_MACRT_Open before the caller uses the driver again.
Precondition
DRV_G3_MACRT_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid instance handle, returned from the driver DRV_G3_MACRT_Open routine. |
Returns
None.
Example
// 'handle', returned from DRV_G3_MACRT_Open previously called DRV_G3_MACRT_Close(handle);
Remarks
None.