1.1.2.4.39 MAC_RT_TX_CFM_OBJ Struct
C
typedef struct {
/* MAC RT Status */
MAC_RT_STATUS status;
/* Flag to indicate Timestamp should be updated */
bool updateTimestamp;
} MAC_RT_TX_CFM_OBJ;
Summary
Contains a transmission result and timestamp.
Description
This structure contains the information of a transmission, its result and timestamp. Possible results are:
- MAC_RT_STATUS_SUCCESS
- If the transmission succeeded
- Frame is transmitted if no ACK is requested
- Frame is transmitted and ACK received back, if ACK was requested
- If the transmission succeeded
- MAC_RT_STATUS_CHANNEL_ACCESS_FAILURE
- If CSMA algorithm finds channel busy for the number of configured backoff retries
- MAC_RT_STATUS_NO_ACK
- If transmitted MAC frame required an ACK back, and after configured MAC retries, the ACK was not received
- MAC_RT_STATUS_DENIED
- If MAC RT is not ready to transmit
- If a transmission is already requested and not yet finished
- If a reset occurs on MAC RT during transmission
- MAC_RT_STATUS_INVALID_PARAMETER
- If any of the parameters in the transmission request contains invalid data
- MAC_RT_STATUS_TRANSACTION_OVERFLOW
- If SPI communication with PLC transceiver fails
Remarks
None.