1.1.2.4.8 DRV_G3_MACRT_InitCallbackRegister Function
C
void DRV_G3_MACRT_InitCallbackRegister(
const SYS_MODULE_INDEX index,
const DRV_G3_MACRT_INIT_CALLBACK callback
);
Summary
Allows a client to set a G3 MAC RT initialization event handling function for the driver to call back when the PLC binary file has been loaded into the PLC transceiver.
Description
This function allows a client to register a G3 MAC RT initialization event handling function for the driver to call back when the loading of the PLC binary file has finished.
This routine should be called before calling DRV_G3_MACRT_Open function.
The callback once set, persists until the client closes the driver or sets another callback (which could be a NULL pointer to indicate no callback).
Precondition
Function DRV_G3_MACRT_Initialize must have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| index | Identifier for the object instance to be opened. |
| callback | Pointer to the callback function. |
Returns
None.
Example
void APP_PLC_Init_callback(bool initResult) { if (initResult == True) { } else { } } DRV_HANDLE handle; DRV_G3_MACRT_initCallbackRegister( DRV_G3_MACRT_INDEX_0, APP_PLC_Init_callback ); handle = DRV_G3_MACRT_Open(DRV_G3_MACRT_INDEX_0, NULL); if (handle == DRV_HANDLE_INVALID) { }
Remarks
None.