AXI4 Initiator/Target Interface in the RTL Interface Report
(Ask a Question)As described in 3.5.1.18 Top-Level RTL Interface, AXI4 Initiator/Target can be used for many different types of interfaces. For example, let's say we have the following top-level function:
#define SIZE 16 int top(int *arg1, int *arg2, int *arg3) { #pragma HLS function top #pragma HLS interface control type(axi_target) #pragma HLS interface argument(arg1) type(axi_initiator) ptr_addr_interface(axi_target) num_elements(SIZE) #pragma HLS interface argument(arg2) type(axi_initiator) ptr_addr_interface(simple) num_elements(SIZE) #pragma HLS interface argument(arg3) type(axi_target) num_elements(SIZE) ... }
The corresponding RTL interface report will be:
+------------------------------------------------------------------------------------------------------------------------+
| RTL Interface Generated by SmartHLS |
+----------+-------------------------------------+---------------------------------+------------------+------------------+
| C++ Name | Interface Type | Signal Name | Signal Bit-width | Signal Direction |
+----------+-------------------------------------+---------------------------------+------------------+------------------+
| | Clock & Reset | clk (positive edge) | 1 | input |
| | | reset (synchronous active high) | 1 | input |
+----------+-------------------------------------+---------------------------------+------------------+------------------+
| | Control via AXI4 Target | axi4target_* | | |
+----------+-------------------------------------+---------------------------------+------------------+------------------+
| arg1 | AXI4 Initiator | axi4initiator_* | | |
| | with ptr_addr_interface(axi_target) | axi4target_* | | |
+----------+-------------------------------------+---------------------------------+------------------+------------------+
| arg2 | AXI4 Initiator | axi4initiator_* | | |
| | with ptr_addr_interface(simple) | arg2 | 64 | input |
+----------+-------------------------------------+---------------------------------+------------------+------------------+
| arg3 | AXI4 Target | axi4target_* | | |
+----------+-------------------------------------+---------------------------------+------------------+------------------+
When the top-level module uses AXI4 Initiator/Target, it will have many axi4initiator_*
/axi4target_*
ports respectively, with varying widths and directions. As a result, the Signal Bit-width
and the Signal Direction
columns for the ports are left blanked. These ports are commonly used by all AXI4 Initiator/Target interfaces of the top-level module.
In the above example:
- 3.5.1.18.1.2 AXI4 Target for Module Control is used. The
Signal Name
no longer showsfinish
,ready
, andstart
as in the case of 3.5.1.18.1.1 Simple Module Control Interface. arg1
andarg2
are AXI4 Initiator Interfaces for Pointer Argument, with the pointer address interface beingaxi_target
andsimple
respectively. These 2 arguments each corresponds to 2 lines in the report, one for the AXI4 Initiator argument itself and the other for the corresponding pointer address interface. Note that for the case ofptr_addr_interface(simple)
, the HLS module will have a simple input port with the same name as the pointer argument (in this example, the port isarg2
) with a well-defined bit-width and direction (64
andinput
in this case).arg3
is an AXI4 Target Interfaces for Pointer Argument, although an argument that's 3.5.1.18.2.2 AXI4 Target for Scalar Argument will also show a similar line.