Description
This Tcl command removes the programmer from the programmer list. Right-click a programmer to Ping, Self-Test, Scan, Check Chain or Remove it from the list.
remove_prg -name { name }
Arguments
| Parameter | Type | Description | 
|---|
| name | string | Specifies the programmer to be removed. You can repeat this argument for multiple programmers. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'name' is missing. | 
| None | The programmer with name 'prg_name' does not exist. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'remove_prg [-name "name"]+' | 
Example
The following example removes the programmer '03178' from the programmer list:
set prg_name "03178"
remove_prg -name "$prg_name"